Other Parts Discussed in Thread: BQ25798
Tool/software:
Hello! I decided to make a new post from the previous thread as we can now successfully communicate with the BQ25798! Just one more problem, it doesn't seem to charge the battery. I have a multimeter connected in series with the battery, and I also have my 5V-3A PSU connected at the input. I know 1 LED draws about 1mA, the chip draws 5ma, and we have 2 LEDs (see the schematic, 1 for STAT and another for 3V3 indication), so 7mA total draw, which is the case! In the GUI it says "Trickle charge" right now, but it doesn't appear to draw ANY current from the PSU, maybe at max 1mA!
Also the STATUS LED now lights up every time I put the CE SHUNT as said in the BQ25798 EVM datasheet, because my board is pretty much a copy of it.
The charger may be seeing my Sodium-Ion battery that I want to charge as dead... Because its voltage range is between 3.95V and 1.5V, now it's at about 2.16. For a Li-Ion that battery would be long dead but this is not the case for us and I suspect it doesn't trigger normal 0.5A charge because of that. So how can I tell it to straight up forget trickle && pre-charge and go to normal charge? What are the settings I should enable/disable? See all the GUI stats and settings bellow:

And the GUI images: