Part Number: BQ25792
Tool/software:
Hi, I'm having some issues with battery charging using the BQ25792.
Specifically the battery does not appear to charge and 0mA are going to or from the battery when I read register REG33_IBAT_ADC, when the charger is reporting that it is in fast charge mode, without faults.
Its a 2 cell battery.
The charging supply is 12V and limited to 300mA.
VBUS reads 12V, VSYS and VBAT read 7V, which agree with voltmeter measures.
IBUS reads 17mA.
An LTC2959 fuel gauge is also being used to monitor current to and from the battery, and it reports a constant discharge current, even while the BQ25792 it is in fast charge mode.
My team mates and I are failing to understand why its not charging and what the cause of the problem is.
Please let me know what further information my team mates and I can provide to assist with the solution.
Thank you.