Tool/software:
Hi Team,
just want to check the actions when batfet is discharging too high current which trigger batocp. Thanks.
BRs
Given
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
just want to check the actions when batfet is discharging too high current which trigger batocp. Thanks.
BRs
Given
Hi Given,
The battery IBAT OCP fault flag triggers if discharge current > 9A min occurs. Because of the battery FET body diode, the BATFET cannot stop the discharge current. If an external shipFET is installed, shipFET present bit (REG0x14[7]) =1 and EN_IBATdicharge_OCP bit (REG0x14[0]) = 1, SDRV charge pump to shipFET gate turns off and shipFET turns off no faster than its turn off time.
Regards,
Jeff