This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: problem with Discharge FET driver line

Part Number: BQ77915

Tool/software:

Hello Iam using BQ77915 to balance cells in a 3 cell battery. When one of the Cell voltage goes below Under Voltage (2.7V), the discharge FET driver line goes low, but when the Cell voltage goes above UV + V hysterisis (2.7+0.8V = 3.5V), the discharge driver line does NOT go high...... What could be wrong?