This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5050-1: Gate drive capability

Part Number: LM5050-1
Other Parts Discussed in Thread: CSD19533Q5A

Tool/software:

Hi Team,

We are planning to use the LM5050-1 controller for an ORing application with the following specifications:

VIn:37V to 54.6V
Iout: 60A continuous 120A peak


We plan on using multiple CSD19533Q5A (3 or 4).

1. Please do suggest if 3 or 4 FET's will suffice or if we need to use more?
2. Will the LM5050-1 be able to provide enough current to drive all these FET's and how can i calculate this? 
3. Will the LM5050-1 be suitable for this specs and application or should we consider using any other ideal diode controller for this application?

Best Regards,
Noel