Other Parts Discussed in Thread: TPS61299, TPS61099, TLV61070A, TPS61299A
Tool/software:
Hello,
We are currently using the TLV61220 in a new battery powered project. We see a similar issue to that reported in the related thread, i.e., with the EN pin set low (EN=0), we see a shut-down current in the region of 10uA in a narrow Vin voltage range of 3.0V to 3.2V. Outside this Vin voltage range (i.e. for Vin bigger than 3.2V and Vin smaller than 3.0V) the shut-down current is about an order of magnitude lower and seems as expected on the basis of the datasheet. With EN set to 0, Vin is slightly larger than Vout.
The related threat mentions an explanation of this behaviour. In order to decide whether we can tolerate this unexpected behaviour in our application, it would be good to understand the explanation of this behaviour. Would you be able to share this explanation?
Thank you very much.
All the best
Peter