This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25887: BQ25887EVM schematic questions

Part Number: BQ25887

Tool/software:

Hi,

I'm looking at the BQ25887EVM and I had a few questions.

1. Are the input and output shunt resistors R1 and R6 necessary for operation? I didn't see the voltage drop across them connected back to the BQ25887

2. What is the purpose of D7 which connects Bat to  SNS_SYS

3. What happens if a load is placed on the battery while it's under charge?

   - When the load is less than the charge current will it continue to charge and is it possible to restart charging after completion to keep battery topped off?

   - When the load is more than the charge current and VBAT > VBATLOWV  will the charge stay in fast charge CC?

4. Can you verify my simplified schematic attached looks good?

2211.output.pdf