This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
HI team,
1. I think the device has shoot through protection at switching FET, how to do this?
2. Regarding the spec, is it tested in each chip when production that minimum voltage input to maximum Iout (VBUS = 3.6V and Iout = 5A)? Or is it guaranteed by IC desgin?
Regards,
Hayashi
Hi Hayashi,
Our devices have varying protections to prevent against unwanted operational modes and are tested to comply with the recommended operating conditions.
Regards,
Jared Baxter
HI Jared,
I know that, but please give a clear statement as TI? Customer's quality team would like those in order to judge the device.
My questions was "which mechanisms to prevent shoot through" and "Is every chips tested with specific condition in boundary (VBUS = 3.6V and Iout = 5A)?".
Regards,
Hayashi
Hi Hayashi,
None of our chargers can be tested on a tester while switching and providing full output power. Full output power is only tested on the bench on a few units. Practically, the input power must be greater than the output power. So to get 5A output with a 4.2V battery and VBUS=3.6V, the charger requires 4.2V*5A/3.6A = 5.83A, which is above the max input current rating of 3.3A. Even at higher input voltages, the WCSP package gets too hot, causing the IC to enter thermal regulation, limiting output power, in all but a very few VBUS to VBAT configurations.
Regards,
Jeff