This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25148: LM25148 chip will not switchV .

Part Number: LM25148

Tool/software:

We were testing the circuit from the previous question. We wanted to check the current control loop, and we adjusted the load slightly, the Buck immediately stopped. There is no switching signal at all on the SW node and nothing from the Gates on either mosfet.  We examined the board itself, no shorts and the opamps and LM chip do not have any visible damage and no shorts to ground. the measurements to ground appear fine.  We are powering with 28V , even into a steady load , there is no switching and the output is 0.042V