This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5145-Q1: DC- DC buck regulation 24V to 12V converter, Load 25A

Part Number: LM5145-Q1
Other Parts Discussed in Thread: LM5145, LM5146,

Tool/software:

Hi team,

I am looking for a design solution for DC- DC buck regulation 24V to 12V converter in one of our Automotive projects.

The input voltage range: 5V to 48V.

The nominal input voltage :24V.

The output voltage: 12V

The Continuous load current: 20A.

The peak load current: 25A

 could you kindly suggest design solution for DC DC Buck converter.

Thanks,

jayanthi.