Other Parts Discussed in Thread: TPS3808
Tool/software:
Hi,
In the datasheet of the TPS3808E device it is written on page 4 under the CT pin description that a capacitor >= 130pF is needed for a user programmable delay.
On page 12 it is written capacitor >= 100pF is needed for a user programmable delay.
What is the correct value?
If it is 100pF, is the device designed to allow a 100pF capacitor on this pin? Means is there an additional tolerance band calculated for the capacitor device?
Or is the limit strictly 100pF?
Thanks and best regards,
Patrick