Other Parts Discussed in Thread: TDA4VH,
Tool/software:
#1. There are two I2C bus on this device, what is their address separately, where specified it in data sheet? or another document?
#2. Which is watchdog I2C bus, seems it is 0x12 from other e2e thread. where described it in datasheet?
#3. How to control the Watchdog, from below command, the offset 0x09 register seems like 409h, if yes, what is mechanism of the register mapping? where described it?
i2cset -f -y 0 0x12 0x09 0xbf
#4. Is the watchdog enabled in default? Why it is not enabled on TDA4VH EVM, but is enabled on customer board, reset every 12 minutes. We found the version are different between VH EVM and customer, what is the difference between them? is there a document?
i2cdump -f -y 1 0x48
#5. How to disable the watchdog from default.