Tool/software:
hello sir,
when we design TPS6594133A-Q1, we have some confused about inductor value. In app note, table 4-1 recommend all inductor value is 220nH.
Powering Jacinto 7 SoC For Isolated Power Groups With TPS6594133A-Q1 + Dual HCPS.pdf
My question is, if we follow below formular to calculate inductor value, there are much different according to actual load current. For example, in 4.4MHz, 0.85V/900mA load current condition, we calculate typical inductor is 586nH, maybe can select actual inductor is 680nH. Much difference compared the recommended value! If follow EVM value 220nH, is the ripple will be much bigger and exceed 20%Iout load current. So, how to understand which one result is correct?