This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Cell balancing

Part Number: BQ76952


Tool/software:

11s1p battery pack

battery cell specification

nominal voltage - 2.3V

standard charge cut-off voltage - 2.8V

standard discharge cut-off voltage - 1.5V

There is a problem with cell balancing at cell voltage below 2V.

When the cell voltage drops below 2000mV during discharge

Cell balancing does not work.

Which part of the setting should I modify?