Tool/software:
Hi,
Greetings.
I am working on 12s BMS using BQ76952. Kindly verify the schematics. the R16 is getting heated up which is connected in series with a diode then to a BJT that connects BREG and REGIN. How to configure REG0, REG1 and REG2 for the above schematics? What could be the possible reason. If there are any other suggestions to change in the schematics, mention them too.
Thank you.