This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55288: TPS55288RPMR: Unable to turn ON using EN pin

Part Number: TPS55288

Tool/software:

Hi,

Thanks for the reply.

I would like to confirm this again

So, even if the EN pin voltage is above 1.15V as recommended in datasheet, we need software support to generate the output.

Is my understanding is correct?

In datasheet it is provided that high voltage at EN pin enables the device.

Could you please explain the working in detail..

  • Hi Maya,

    So, even if the EN pin voltage is above 1.15V as recommended in datasheet, we need software support to generate the output.

    Yes.

    In datasheet it is provided that high voltage at EN pin enables the device.

    When EN is high, VCC supply is enabled and the I2C is ready for communication. Need OE bit to enable it.

    Regards,

    Mulin