Other Parts Discussed in Thread: AM3352, , TPS65218
Tool/software:
Hello,
I designed a circuit using this PMIC to power an AM3352BZCZ30 solution along with the DDR3L and eMMC necessary for normal use.
After testing the circuit I can't power on the PMIC - at this point I have no FW on the AM3352 so the PWR_EN is pulled up, but from what I saw on the datasheet state machine (Figure 8-34) that shouldn't be necessary.
I'm betting on some detail that I must be missing from the design. I followed the advice from the datasheet and grounded the AC pin (the application of the board should power the PMIC immediately the moment external power is connected to it). I figured it may be due to having a floating PB pin and put a 100k pull up on it but it didn't solve the issue.
I'm re-reading the datasheet trying to find something that may be out of place, but can't seem to find the issue so far. Can you give me some help?
Bellow I attached the schematic I have implemented, to get your opinion. Thank you in advance.