Tool/software:
Hi,
I would like to confirm if the ideal diode controller LM7480-Q1 can be used for 48V automotive systems?
I have referred the datasheet LM7480-Q1 Ideal Diode Controller with Load Dump Protection datasheet (Rev. C) and planning to use the circuit as per figure 10-25 application diagram.
Could you please clarify the below points.
1)I need input reverse battery protection of 52V.This means the diode D4 in figure 10-25 needs to be replaced. What is the voltage rating required for D4 in this case.
2)Transient voltage (Load dump) at input can go up to 70V for 40ms.Will this circuit able to meets this?
3)Input voltage nominal range is 36-52V but shall go up to 60V for 1hour.Will this be okay if I chose D1 of 60V.
4)In the datasheet example Q1 is chosen for 200V Mosfet (I understood this is for load dump protection) whereas Q2 is rated for 60V.Whys is it so?
Thanks and Regards,
Reshma