This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
Customer now are evaluating TPS62A01A now, Could you please also help to test below application usage?
Input voltage:3V
Output voltage:2.7V
Inductor: 2uH
Output capacitor:10uH
They want the efficiency curve from 10mA to 1.5A and the ripple in 1A
Thank you,
Yishan Chen
Hi Yishan,
Thank you for using E2E,
Inductor: 2uH
For the customer operating conditions, VIN = 3V & VOUT = 2.7V, the recommended L = 1uH & C =10uF. If the customer would like to go beyond the datasheet recommendation, then the stability of the device need to checked using bode plot measurements.
Thank you & regards,
Moheddin.
Hi Moheddin,
Customer is still insisting used 2uH inductor.
Could you please help to test the efficiency curve from 10mA to 1.5A, and the ripple at 1A with 2uH inductor.
I will send customer and the detail for this opportunity through Email.
Best Regards,
Yishan Chen.
Hi Yishan,
As we are already discussing in the email, can you please close the thread here.
Thank you & regards,
Moheddin.