Tool/software:
Dear Expert
Use UCC14141 and UCC21755. UCC21755 requires VDD to add at least 10uF to COM. For UCC14141, when the capacitance between VDD-COM is 10uF, VEE-COM needs to add 50uF.
The current question is whether the capacitance between UCC21755 VDD-COM can be reduced to 2.2uF. There is still 2.2uF near UCC14141, and an additional 10uF will be added near UCC21755 VDD-VEE? Configure as shown in the following figure
Drive frequency 70kHz, Qg 600nC.