This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2660: Supply Line Interrupts

Part Number: TPS2660


Tool/software:

Hi TI Team

We use the TPS26601 in a new system. But we have to make our system capable of handling interrupts on the supply. There is a thread talking about putting a resistor in series with the capacitor on the dVdT pin. So if im correct the voltage on the dVdT Pin is about VOUT/24.5. My UVLO is set to 15V. So I need the Voltage on this pin (capacitor) to stay above 0.6V on an interrupt to make the TPS26601 not asserting the nFLT Pin and go into ramp control mode?

Thank you in advance!

Regards Theo