Part Number: LM5109B
Tool/software:
I am using 3 LM5109BMAX/NOPB in an automotive VFD application.
The MOSFET Module is an On-Semi NXV08V110DB1.
My driver circuit looks like this:

I think I have met all the requirements from the datasheet,
- VDD is between 8 and 14 Volts - a Voltage regulator takes care of that.
- HS is between -1 and 90 Volts, my DC-Supply is limited to 60 Volts, usually the DC Bus is set to 12 - 15 Volts ...
- HO and LO are clamped against negative voltages
except one, i don't know hot to make sure HB to HS stays within the limits:

Chapter 7.5 "HS Transient Voltages Below Ground" says:
In the application, the HS node is clamped by the body diode of the external lower N-MOSFET, therefore the HS voltage will generally
not exceed –1 V. However in some applications, board resistance and inductance may result in the HS node exceeding this stated
voltage transiently. If negative transients occur on HS, the HS voltage must never be more negative than VDD – 15 V. For example, if
VDD = 10 V, the negative transients at HS must not exceed –5 V.
How can I make sure that HB stays within it's limits?
If I'd try to enforce that with a 12 Volt Zener Diode from HS (Anode) to HB (Cathode), I'd literally connect the Motor Phase with the Driver Supply. That sounds like a really bad idea to me?
Is there anyone who has a practical advice for me, how this can be achieved? Thank you very much