Tool/software:
Hi there,
I'm trying to use the TPS552892 in my application with specifications Vout = 12V, Vin = 8-24V, and Iout = 2A. I have copied many of the values from the evaluation module TPS552892EVM-111, but I am still running into some issues with lower Vin at a higher output current.
I am using a programmable DC electronic load, which should be resistive. With Vin = 8V and currents above 750mA or so, the output turns into a triangular wave. With higher Vin, even still in boost mode, it is able to handle more load (I haven't characterized this relationship too carefully). I played a little with output capacitance and it helped some stability issues at even lower load currents, but did not help at 750mA.
I then tried using the programmable load with the evaluation module. The EVM does better than my board, but still seems to fail its own specs. With Vin > 6V it should be able to handle 3A. However, when I set Vin = 8V and Iout = 1.5A, the output produces a triangular wave similar to what I saw with my own board. I measured the following waveforms on the scope:
Ch1(yellow) = Vout, Ch2(blue) = SW1, Ch3(red) = SW2
Using Vin=8V, Iout=1.2A:
Using Vin=8V, Iout=1.5A:
(Note the timescale is very different in the two images). Changing Vin and Iout create different versions of these two waveforms. The patterns make sense in the working conditions, but I'm not sure what is happening when it's failing at the higher loads. At 1.5A it's still able to hit 12V for a little bit of time, but as Iout increases it stops hitting 12V and turns into a triangular wave. I thought it might be a pattern that's familiar to somebody who has more experience with switching regulators.
I'm hoping to use this as a clue to troubleshoot my own design, since it seems to be failing in the same way (just at a lower load than the EVM). But since the EVM should work to its rated spec, I'm not sure if there is something else wrong with my setup.
Thanks!