Other Parts Discussed in Thread: UCC27288, , UCC27289, UCC27284-Q1, LM25145, UCC27624, UCC27614
Tool/software:
I am designing a full H-bridge circuit with an output voltage (V_DS) of +1.6V and an output current ranging from 5 to 8A. The load is connected between two H-bridges. I have considered using the UCC27211 gate driver IC, and I have also looked into other ICs such as the UCC27284-Q1, UCC27288 3-A and UCC27289. However, I am uncertain if these can effectively drive the MOSFETs I am using. The voltage changes direction between +1.6V and -1.6V by controlling the full bridge switches. In one case, the current flows from S1 to the load and then to S4, and in the second case, the load current moves from S3 to the load and then to S2.
Could you recommend which driver IC would be more suitable for my requirements?