This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
Where can I download the TPS65994AE Technical Reference Manual? I currently try to get the IC running on our board, but the 5V output remains at 0V...
Besides, I currently use the Application Customiozaton Tool rel. 6.4.32 with an AArdvark adapter.
It seems that the Flash read/Flash write ops are corrupted (the commands apply to a SPI interface??). When I read back an EEPROM, I get a 1Mbyte file filled with all 0's, though I'm sure the EEPROM is not filled with 0's.
Is there a more up to date release of this tool?
Regards
Hi Tommy,
It seems that I cannot get the document : Access denied and I dont know why??? I already made a request to get all related documentation on the TPS 65994AE since september and I still wait but nothing happens.
Can you escalated this problem to the guys responsible of this IC so that I can finalize my design please?