Other Parts Discussed in Thread: TPS25750
Tool/software:
Hi team,
When use TPS25751 as OTG source, supoort 5V/3A, 9V/3A, 15V/3A, 20V/5A.
Does the PP5V path need to support the 5V/3A output capacity? And PPHV support the others?
Based on following post, I though the answer is yes.
However, based on the following TI design, PP5V only get 300mA/5V power capacity, and it support 5V/3A, 9V/3A, 15V/3A, 20V/5A. So it seems PP5V is not necessary for 3A capacity.
https://www.ti.com/tool/PMP41062
The PP5V power capacity is confused to me 3A or 300mA, could you help clarify the power capacity of PP5V?
Thanks and Best Regards,
Will