Other Parts Discussed in Thread: TPS552892, TPS552882
Tool/software:
Hello
I would like to use TPS61288 boost for my system which is battery operated with 3 cells. Below are the requirement specifications.
Vin_min = 10V and Vin_Max = 15V.
Vout = 15V and Iout = 4A.
for this requirement TPS61288 will it support. if yes what are the design constraints has to be considered for 4A continuous current.