Tool/software:
Hi,
The Shutdown command is not working both by sending two time the Shutdown command to a Sealed Gauge within 4 seconds and by unsealing and sending the command. Normally all Gauges go into shutdown mode after I send the commands, but some batteries do not go into Shutdown mode. There is also no electrical connection PACK pin so the voltage is not the root cause. Is it possible that the atatched log file can be reviewed to identify the root cause?
Thu Oct 17 11:32:17 CEST 2024 Device Version Info = 4500_2_11 BQZ Device Name = bq40z50R2 BQZ Firmware Version = V2_11_BLD52 Design Capacity = 7200 Design Voltage = 11100 Specification Info = 0x0031 Manufacturer Date = 2024-8-22 Serial Number = 0x0222 Manufacturer Name = Philips Device Name = 958231 Device Chemistry = LION Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,MaxTurboPwr,SusTurboPwr,MaxTurboCurr,SusTurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,vBAT,vPACK,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellPower1,CellPower2,CellPower3,CellPower4,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,GaugeTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,NoLoadRemCap,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,CompRes1,CompRes2,CompRes3,CompRes4,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,QMax1,QMax2,QMax3,QMax4,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,CBTime1,CBTime2,CBTime3,CBTime4,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus 1,2024-10-17 11:32:21,4.007,0x6381,710,10,0x0001,0,65535,65535,1,26.7,10594,0,0,1,24,24,1669,6971,65535,65535,65535,0,0,0x00C0,1,-13684,-12555,-16099,-14400,97,0x6381,0x0001,0x08,0x0002,0x50,0x0814,0x03F8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3531,3531,3531,0,10585,6259,0,0,0,0,0,0,0,0,0,0,24.5,26.7,26.4,195.0,196.7,26.7,24.5,26.7,1669,1667,6971,7617,1934,1669,1667,5302,5950,6971,7617,26.4,26.4,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,516,12624,12640,12640,0,0,0,2,2336,2212,2272,0,8443,8465,8467,0,0,0,0,0,0,2,5.71,18000,12624,12640,12640,0,10800,533,0,0,12624,12640,12640,0,16384,6993,7638,1155,SUCCESS 2,2024-10-17 11:32:25,8.014,0x6381,710,10,0x0001,0,65535,65535,1,26.7,10594,0,0,1,24,24,1669,6971,65535,65535,65535,0,0,0x00C0,1,-13684,-12555,-16099,-14400,97,0x6381,0x0001,0x08,0x0002,0x50,0x0814,0x03F8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3531,3531,3531,0,10582,6260,0,0,0,0,0,0,0,0,0,0,24.5,26.7,26.4,196.5,196.7,26.7,24.5,26.7,1669,1667,6971,7617,1934,1669,1667,5302,5950,6971,7617,26.4,26.4,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,520,12624,12640,12640,0,0,0,2,2336,2212,2272,0,8443,8465,8467,0,0,0,0,0,0,2,5.71,18000,12624,12640,12640,0,10800,533,0,0,12624,12640,12640,0,16384,6993,7638,1177,SUCCESS 3,2024-10-17 11:32:29,12.015,0x6381,710,10,0x0001,0,65535,65535,1,26.7,10594,0,0,1,24,24,1669,6971,65535,65535,65535,0,0,0x00C0,1,-13684,-12555,-16099,-14400,97,0x6381,0x0001,0x08,0x0002,0x50,0x0814,0x03F8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3531,3531,3531,0,10584,6260,0,0,0,0,0,0,0,0,0,0,24.5,26.7,26.4,196.5,195.6,26.7,24.6,26.7,1669,1667,6971,7617,1934,1669,1667,5302,5950,6971,7617,26.4,26.4,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,524,12624,12640,12640,0,0,0,2,2336,2212,2272,0,8443,8465,8467,0,0,0,0,0,0,2,5.71,18000,12624,12640,12640,0,10800,533,0,0,12624,12640,12640,0,16384,6993,7638,1176,SUCCESS 4,2024-10-17 11:32:33,16.018,0x6381,710,10,0x0001,0,65535,65535,1,26.7,10594,0,0,1,24,24,1669,6971,65535,65535,65535,0,0,0x00C0,1,-13684,-12555,-16099,-14400,97,0x6381,0x0001,0x08,0x0002,0x50,0x0814,0x03F8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3531,3531,3531,0,10584,6258,0,0,0,0,0,0,0,0,0,0,24.5,26.7,26.4,196.3,196.5,26.7,24.5,26.7,1669,1667,6971,7617,1934,1669,1667,5302,5950,6971,7617,26.4,26.4,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,528,12624,12640,12640,0,0,0,2,2336,2212,2272,0,8443,8465,8467,0,0,0,0,0,0,2,5.71,18000,12624,12640,12640,0,10800,533,0,0,12624,12640,12640,0,16384,6993,7638,1142,SUCCESS 5,2024-10-17 11:32:37,20.018,0x6381,710,10,0x0001,0,65535,65535,1,26.7,10592,0,0,1,24,24,1669,6971,65535,65535,65535,0,0,0x00C0,1,-13684,-12555,-16099,-14400,97,0x6381,0x0001,0x08,0x0002,0x50,0x0814,0x03F8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3531,3531,3531,0,10584,6260,0,0,0,0,0,0,0,0,0,0,24.6,26.7,26.4,196.7,195.7,26.7,24.6,26.7,1669,1667,6971,7617,1934,1669,1667,5302,5950,6971,7617,26.4,26.4,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,532,12624,12640,12640,0,0,0,2,2336,2212,2272,0,8443,8465,8467,0,0,0,0,0,0,2,5.71,18000,12624,12640,12640,0,10800,533,0,0,12624,12640,12640,0,16384,6993,7638,1155,SUCCESS 6,2024-10-17 11:32:41,24.033,0x6381,710,10,0x0001,0,65535,65535,1,26.7,10592,0,0,1,24,24,1669,6971,65535,65535,65535,0,0,0x00C0,1,-13684,-12555,-16099,-14400,97,0x6381,0x0001,0x08,0x0002,0x50,0x0814,0x03F8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3531,3531,3531,0,10584,6259,0,0,0,0,0,0,0,0,0,0,24.5,26.7,26.4,196.0,195.6,26.7,24.5,26.7,1669,1667,6971,7617,1934,1669,1667,5302,5950,6971,7617,26.4,26.4,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,536,12624,12640,12640,0,0,0,2,2336,2212,2272,0,8443,8465,8467,0,0,0,0,0,0,2,5.71,18000,12624,12640,12640,0,10800,533,0,0,12624,12640,12640,0,16384,6993,7638,1158,SUCCESS 7,2024-10-17 11:32:45,28.040,0x6381,710,10,0x0001,0,65535,65535,1,26.7,10592,0,0,1,24,24,1669,6971,65535,65535,65535,0,0,0x00C0,1,-13684,-12555,-16099,-14400,97,0x6381,0x0001,0x08,0x0002,0x50,0x0814,0x03F8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3531,3531,3531,0,10584,6256,0,0,0,0,0,0,0,0,0,0,24.5,26.7,26.4,196.5,196.7,26.7,24.5,26.7,1669,1667,6971,7617,1934,1669,1667,5302,5950,6971,7617,26.4,26.4,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,539,12624,12640,12640,0,0,0,2,2336,2212,2272,0,8443,8465,8467,0,0,0,0,0,0,2,5.71,18000,12624,12640,12640,0,10800,533,0,0,12624,12640,12640,0,16384,6993,7638,1122,SUCCESS 8,2024-10-17 11:32:49,32.047,0x6381,710,10,0x0001,0,65535,65535,1,26.7,10592,0,0,1,24,24,1669,6971,65535,65535,65535,0,0,0x00C0,1,-13684,-12555,-16099,-14400,97,0x6381,0x0001,0x08,0x0002,0x50,0x0814,0x03F8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3531,3531,3531,0,10585,6260,0,0,0,0,0,0,0,0,0,0,24.6,26.7,26.4,195.7,196.5,26.7,24.6,26.7,1669,1667,6971,7617,1934,1669,1667,5302,5950,6971,7617,26.4,26.4,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,544,12624,12640,12640,0,0,0,2,2336,2212,2272,0,8443,8465,8467,0,0,0,0,0,0,2,5.71,18000,12624,12640,12640,0,10800,533,0,0,12624,12640,12640,0,16384,6993,7638,1367,SUCCESS
Thanks and regards,
-Enrique