This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61023: Strange power dips during operation with TPD61023DRLR

Part Number: TPS61023
Other Parts Discussed in Thread: TPS60123,

Tool/software:

Hi,

I have a circuit using a TPD61023DRLR to generate 5V from two AA cells in series.

I'm testing the circuit using a poer supply varying the voltage to check operation and I've been getting crashes randomly at voltages below 2.2V

The circuit uses an ESP12F

The TPS60123 is configured

I have 100uF MLCC across the supply pins (Vbatt) and the 5V goes to a 3.3V LDO to supply the ESP.

C7 21 and 22 are Mulilayer ceramic capacitors.

I have monitored the 5V and 3.3V with an oscilloscope and found the following, the Blue trace is the 5V form the TPS61023

Do you have any suggestions as to what it could be and how to fix it.

PCB layout

This is a scope trace after adding an extra 22uF MLCC across the 5V (Yellow) also I've added the SW pin (Blue) to the Scope trace as the 5V glitch occurs