Tool/software:
I wanted to understand what the requirement for using the BQ76952 chip for a BMS that needs to go through UL1998/991(IEC60730) certification vs using the BQ76952. Can the BQ76952 pass this certification and what features would the BMS need to have enabled to allow it to pass this function safety certification.
What are main differences between the two chips and the reason the BQ79656 is functional safety certified and the BQ76952 is not?