This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62442: output current capability

Part Number: TPS62442

Tool/software:

Hi Expert,

From the datasheet and other E2E threads, looks like each channel of the TPS62442 can output 3A, the sum of the two channels' current needs to be less than 4A, right? However, I would like to know, is the total current limited to 4A due to thermal limitations? If the heat dissipation conditions are good, can it support two 3.3V to 1.2V/2.5A? 

Regards,
Hailiang