This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5410-EP: Cannot calculate inductor rms current and peak current

Part Number: TPS5410-EP


Tool/software:

Is there an issue with equations 5 and 6 in the datasheet for this IC? I cant seem to get values that make sense (peak current less than my desired output current). Am I doing this wrong? Or is there possibly another way to verify those two values before selecting an inductor? My values are seen below:

Thank you

Vout [V] 5
Vin(max) [V] 30.5
K_IND 0.3
I_OUT [A] 0.5
F_SW [Hz] 500000
L_MIN [H] 6.96721E-05