Other Parts Discussed in Thread: BQ34Z100-G1, BQ34Z100
Tool/software:
Hi TI Team,
We have recently initiated a new 48V battery project, utilizing the BQ76952 and BQ34Z100-G1 ICs on the same BMS board. The pack charge current is 240A continuous, and the discharge power is approximately 1200W (around 30A). Due to the significant difference between charge and discharge, we have separated the charge and discharge paths.(high side drive)
Given the high power dissipation on the sense resistor when using a high-value resistor, we are considering using a resistor value between 0.1 to 0.25 milliohms based on the thermal calculations of the pack. In our previous project, we used a 0.5 milliohm resistor with the same ICs and did not encounter any issues related to calibration, noise, or measurement tolerances.
Could you please advise if there are any potential risks associated with using a resistor as low as 0.1 milliohms in terms of SoC accuracy, measurement errors/tolerances, and noise?
Thanks