This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28881: Isolated flyback design - troubles with output power - following

Part Number: UCC28881


Tool/software:

Hello, lets continue with closed topic: UCC28881: Isolated flyback design - troubles with output power. Sorry for my delay caused by my injury. 

I have tried 760301306 Wuerth transformer, which has a 1.8mH and circuit behaved same way. I have tried also 2 primary windings in series so Lpri was around 3.6mH (checked by RLC meter) and secondaries were also in series. This option was tested just to see what happens when Lpri will be as you reccomended.This connection had a same limiting behavior. Oscillograms are attached. 

Please let me know your opinion. 

I have also tried Pulse PH9385.011NLT 3.2mH transformer, but it was not able to reach output parameters. 

I'm testing pulse transformers, which maybe does not have ideal parameters for this kind of source. But I'm really struggling with the room for transformer. I need to keep it so small as possible (max. width 11mm and length 18mm). If you have any recomendation for transformer or combination with another IC, I would be also happy. 

BR Zdenek