This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2116: Current is drawn from VIN1 even if VIN2 is active

Part Number: TPS2116

Tool/software:

In my design I'm using the TPS2116 to switch between two voltage sources (A DC/DC 24V --> 5VDC) Voout is connected to a DC/DC 5V ->3.3V

VIN1 = +5.3V

VIN2 = +5.0V


The TPS is set to run in Priority mode (MODE pin is connected to Vin1)
The PR1 pin is connected to a resistor divider 17,8k /5,6k

Scenario

  1. 50mA load connected to +3.3V 
  2. Both supply is active
  3. Current is drawn from VIN1 (0 from VIN2)
  4. Supply1 (VIN1) is deactivated
  5. Current is drawn from supply 2 (0 from VIN1)
  6. Supply1 (VIN1) is activated
  7. Current is drawn from VIN1 (0 from VIN2)



Everything works as expected, repeating the same scenario but increasing the load to 250mA, causes the VIN1 to draw a small current when its activated again (Step6 & 7), VIN2 still draws the major of the current

Reseting VIN2 (deactivate and then activate) "resets" the issue -> VIN1 draws all the current.

Any ideas what causing this?