Other Parts Discussed in Thread: BQ25792, , TPS25751
Tool/software:
IN our config, we supply power via tow different source, to the BQ25792. One of those sources is a 12V supply. The other source is the '750.
We have Vin_3V3 connected to the PCBA 3.3V rail.
If the '750 doesn't see a USB-C signal, and no power on VBUS, then the device reports always in PTCH mode. If we connect a USB-C PD to the '750, then the firmware loads from the EEPROM, and the device goes to APP mode.