Tool/software:
Hi Expert,
Which should We adopt for Rtt, the value displayed on WEBNECH or the value calculated using Equation 3 in D/S?
For example
When We initiate WEBENCH with the settings VOUT=3.3V, VIN=5V+/-5%, IOUT=3A Ta=40, the value of Rtt is displayed as 4.32k by default.
On the other hand, when we substitute VOUT=3.3V, COUT=100uF, KTT=1.8(same as WEBENCH) into Equation 3, As a result of the calculation, the value of Rtt is 9.88k.
It seems that the value of Rtt is different.