This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Rtt values can be either calculated or found in the selection table, while most of them are not standard values. Is it necessary to use multiple resistors to get the exact value or just pick one close to this value?
Btw, does Rtt have any requirement on power rating? I didn't find such information in pth datasheets.
The RTT value when calculated should be = to or slightly greater then the calculated resistance.
The current in the RTT is in high micro amps. Any wattage resistance can be used for Rtt statring with 0201
Tom