Part Number: UCC28950
Tool/software:
Hi,
The error amplifier output Comp pin is 0.25~4.25Vdc per specs. In the application, I measured the voltage very unstable. Refer to attached slide 1 and 2, yellow trace is the measured Comp pin. The AC/DC power supply output voltage drops from nominal 36Vdc to ~16Vdc. I suspected the drops caused by the ripple because the Comp pin voltage is stable when the AC/DC power supply is loaded with Electronic load (slide 3).
Questions: Is it normal for Comp in to be unstable but within 0.25~4.25Vdc range?
Thanks
Brian