This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I calculated the thresholds of UVLO and OVP according to the equations UVLO (6) and OVP (7).
I think there are some issues:
UVLO:
In equation (6), there is a mistake to calcuate R2. I think in formular there should be Vpwr instead of Vpwr_off. If I change equation, the values will match with the example.
Please can you check this?
OVP:
The functional block diagram does not match with the figure 23 "Basic OVP Configuration". The comparator pins + and - are swapped.
If I add the values from the example, I calculate Vpwr to 82.583V and Vhys to 2V, so the turn back voltage is 80.583V.
Please can you check both calculations and provide the corrected one.