Other Parts Discussed in Thread: GPCCHEM, GPCCEDV
Tool/software:
Hi,
I previously generated a golden image using the BQ34110 EVM for a 1500mAh battery. Now, the battery capacity has been upgraded to 2000mAh, with the same manufacturer and battery type. My plan is to flash this golden image onto the fuel gauge, update the "learned full charge capacity" parameter from 1500 to 2000 for the new battery, generate a new golden image, and use it for the 2000mAh battery. Do you think this approach would work?
Since only the capacity has changed and the other specifications remain the same, So I would value your expert opinion.
Sharing datasheet of both batteries:
2235.1500 mAH Battery.pdf18650-3.2V-2000mAh电池规格书 - 副本 (2) - 副本 - 副本.pdf
Thanks,
Parth