This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25730: Does input current include system current?

Part Number: BQ25730


Tool/software:

I'm working on a board that's intended to be a scaled-up version of a product I've already designed. Unfortunately, the scaled-up version has a lot more peripherals and a more powerful CPU, so it requires 17A max as opposed to just 10A to run the system and charge the battery simultaneously. The battery specifications are the exact same. Can I keep using the BQ25730 in this case? Or do I need to find one with an input current limit above the combined current draw of the charger and the system?