Tool/software:
I tried to power up the board with the following conditions:
1. At no load condition.
a. Tied PFM pin to VDD so that board works in PFM mode at light load and VCCX to GND.
b. Input voltage is set to 48V with current limit = 0.1A
Observations:
1. Output voltage = 2V.
2. VCC = 5V.
3. EN voltage = 8.5V
4. PG = 0.175 mV.
Can anyone let me know why PG is getting pulled down. If anyone has faced similar issue, please let me know how to debug it?