This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2HCS10-Q1: OL_ON_CH1 / OL_ON_CH2 is not detected, when Output is active and open load is created.

Part Number: TPS2HCS10-Q1


Tool/software:

---------------------------------- OL_ON -----------------------------------------------------

DIAG_CONFIG_CH1 Configured with the value of 0x4602 to detect the OL_ON Detection

Load is connected to CH1,

Load is activated by writing SW_STATE Register 

Load Draws around ~1200mA

Create the OPEN load.

Read the CH1 Fault state using the FLT_STAT_CH1,

OL_ON_CH1 Bit is not SET

Would you please help me with this? Am i missing any Register Configuration ?