This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7481-Q1: Mosfet SOA margin calculator tool

Part Number: LM7481-Q1

Tool/software:

Hi team,

The customer found that in this post we recommended the customer to use this tool. I would like to confirm with you whether TI recognizes the authenticity and reliability of this tool.
If it is authentic and reliable, can you explain the judgment basis and logic of the table?

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1370795/lm7481-mosfet-failure

https://www.ti.com/tool/download/FET-INRUSH-SOA-CALC/REV-B

  • Hi Alan,

    FET SOA stress calculation  

    A more detailed explanation of SOA calculation is specified in section 2.3 Understanding MOSFET’s Stress Limitations of Robust Hot Swap Design App note.

    For your understanding below is a step-by-step procedure (extracted from the app note),

    1. Calculate the power stress on the FET during startup. Refer to section ‘2.3.3 Checking SOA for Non-Square Power Pulses’ of the app note.

             Derive t2. Approximation here is that the FET is stressed for a power loss = P2 = PMAX for t2 duration.

              

    1. Now, estimate SOA the FET can handle for t2 This value will be at room temperature. Refer to section ‘2.3.2 Checking SOA for Intermediate Time Intervals’ of the app note.

         

            Remember that the SOA value in the table below needs to be taken at VDS = VIN(max) in the SOA curve of the FET.

           

    1. Now, De-rate the SOA calculated in the above step for the Max operating junction/ case temperature of the FET. Refer to section ‘2.3.1 MOSFET SOA Curve and Thermal Model’ of the app note.

           

          This value can be taken as the temp. of the FET at max load condition,

          

    1. You can consider that the FET has strong SOA if

             SOA(TC) > 1.2 x (P2 / VDS)

             Where,

             SOA(Tc) is from step 3

             P2 is from step 1

             VDS = VIN(max)

             The factor 1.2 is taken to include a 20% margin.

    Regards,

    Shiven Dhir

  • Hi Shiven,

    I have questions about the two formulas, could you please help explain how they were derived?

    Thanks a lot !

    Regards,

    Hao

  • Hi Hao,

    Tstart has been computed from capacitor equation of I =Cdv/dt 

    Where marked box is average of power limiting and current limit mode during startup.

    Second equation is derived as such.

    Regards,

    Shiven Dhir

  • Hi Shiven,

    Thanks for your reply!

    I am wondering why  , How was this formula obtained?

    Regards,

    Hao

  • Hi Hao,

    The SOA curve follows a straight line in a log-log plot. Which can be estimated using a standard power function.

    This is used to find SOA at difference time intervals which are not usually mentioned in the FET datasheets.

    Regards,

    Shiven Dhir

  • Hi Shiven,

    I have got it. Thank you very much!

  • Hi Shiven,

    I am a bit confused about this part.

    I  think converting the triangle into a rectangle is too conservative.

    The equivalent curve assumes that the power limit is the same when VDS changes, but in fact, during the startup process, VDS is decreasing and the corresponding power limit is increasing. Is it because there is no better equivalent solution?

    Regards!

    Hao

  • Hi Hao,

    Yes, triangle has been converted to a rectangle, but the time of stress has also changed. This is the closest equivalent solution.

    Regards,

    Shiven Dhir

  • Hi Shiven,

    I have a question about the calculation tool. It seems that the tool only mentions the impact of output capacitance, but in fact, the output is generally π-type filtering. Will this inductor have an impact in the calculation?

    Regards!

    Hao

  • Hi Shiven,

    I will put you in the discussion email with Harman, TI global, please help share your views on the current issues Harman is facing.

  • Hi Alan,

    I replied over email.

    Regards,

    Shiven Dhir