Tool/software:
Hello.
I have two questions about LM2596T-ADJ/NOP.
1. When using without heat sink, can we use the value of RθJC(top) “2°C/W” for the calculation of Tj?
2. Does RθJC(top) refer to the position shown in the figure below?

3. Should the case temperature be measured at point A or point B?