Tool/software:
Hi sir,
I am testing application using LM5118.
I am using 5milli ohms current sense. the input is 24V and output is 12 volts .
now The full load current is 10A. But till 6A its working fine but as soon as I enter 7A load from No Load. Its going to some kind of protection that the output goes to zero and recovers after 160milli seconds with full load.
cramp is 470pF, CSS = 100nF . L OUT IS 5.6A. OUTPUT CAPACITOR IS 220uF.
IT WILL BE HUGE HELP IF THIS ISSUE IS SOLVED THANKS.