Other Parts Discussed in Thread: BQ77216, TIDA-010208
Tool/software:
We are planning to develop a scalable battery system.
This means we want to have a ‘standard’ module with 14S, each with a BQ76952. Each module should have a slave BMS, so to speak.
In order to be able to vary the capacity of the battery, we want to connect between 1 and 4 of these modules in parallel.
The question would now be, is it possible to operate several BQ76952 in a parallel configuration?
If it is possible, what do we need to bear in mind?
I also have a question about your reference design TIDA-010208: Why is a BQ77216 also used here? The BQ76952 would also be able to trigger a fuse. In other words, when is it necessary to use a BQ77216 and when could it be omitted?