Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

TPS25751: External Mosfet version turns off sourcing after a few seconds

Part Number: TPS25751
Other Parts Discussed in Thread: BQ25731, PMP41013

Tool/software:

Hi,

I am using the TPS25751 for a 4S battery powered USB-PD application. At first, I was using the TPS25751D (internal MOSFET) version and everything worked fine, both source and sink. Due to supply shortages, we had to redesign using the TPS25751S (external MOSFET) version. We kept the schematic exactly the same, but added the two external MOSFETs as needed. While sink is working correctly, sourcing is not. When I try to charge some smartphones, some will start charging and than cut the charging current to zero after a few seconds. This was not happening with the TPS25751D. I have attached the json file I am using together with two short videos, one showing the smartphone charging on the TPS25751D (no issues) and the other showing the same smartphone charging using the TPS25751S where the issue is happening. What can cause such an issue? Is it something in the TPS25751S chip? (maybe INDPM setting is not being correctly set in the TPS25751S memory?)

Note: As you can see in the videos, I am using a USB-PD analyser. If I turn off the PD coms in the analyser, the smartphones enter PPS mode and this always works fine, as I see the source voltage smoothly rising up until its settles and current keeps flowing. The issue is when it smartphone directly negotiates 9V.  Also, the TPS25751 keeps on trying to apply charge until at one point it manages and works. 

As a side note the following are the smartphones tried (note that all had no issues when using the TPS25751D)

Samsung Galaxy A23: negotiates 9V, current immediately reaches about 1.5A, than drops to zero after few seconds.

Xiaomi Redmi note 9 pro: Same as the Samsung

Google Pixel 7: worked without issues. 

Vids and JSON.zip