Other Parts Discussed in Thread: LM70860, LM70880, LM5148, LM5085, LM5137
Tool/software:
Hi Team
do we have any POL solution which can support below spec?

BRs
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brian,
The LM70860 or LM70880 can be paired up as a multi-phase solution to provide the output current that is required. The issue will be the output capacitor load. The LM708X0 has internal soft-start of only 2.8ms (typ) which is quite short to charge up output capacitances for both cases. How about a controller?
Ben
Hi Ben
appreciate your great support here
could you also provide controller solution? it will be good if you can also provide MOS solution.
BRs
Brian